Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
discretepower-vs-module-slide4

The output capacitor selection is also a critical part of the design. The output capacitance determines the load transient performance of the power supply. The output capacitance is required to minimize the voltage overshoot and ripple present at the output of a step-down converter. Poor load transient performance or instability is often caused by insufficient output capacitance, and large voltage ripple is caused by insufficient capacitance as well as a high equivalent series resistance (ESR) in the output capacitor. The maximum allowed output voltage overshoot and ripple are usually specified at the time of design. Thus, to meet the ripple specification for a step-down converter circuit, designers must include an output capacitor with enough capacitance and low ESR.

PTM Published on: 2015-10-16