Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
PowerStor Supercapacitors Slide 10

With the five basic formulas and the four basic parameters needed, the designer can look at some real world examples. The first example is using a Constant Current Application. To start the designer will initially ignore the ESR effect on the voltage drop to get an estimate on the capacitance and then use equation 3 to verify if the size picked will work with the ESR effect. Equation 6 is created by removing the ESR portion and rearranging the equation to solve for capacitance.

PTM Published on: 2011-08-23
PTM Updated on: 2021-09-30