Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Slide 31
Slide 32
Slide 33
Product List
Now the training module will shift its focus to how these fit within a secure system environment. At the most basic level, a client security IC is talking to the host microcontroller. In this scenario, the host algorithm and host keys, or secrets, are implemented in the software by the host microcontroller. Software solutions are not as secure as hardware solutions. In order to address the issue of host key storage, Microchip offers an optional host security IC, which securely stores and manages the host secrets. Each of Microchip’s families offer both the client and host hardware security ICs necessary to implement a truly secure system solution. CryptoMemory® provides this on the client side, CryptoCompanion™ provides this on the host side, and CryptoAuthentication™ client and host IC solutions add another contact solution option. Finally, where there is a need for a secure RFID implementation, Microchip offers a full solution with CryptoRF®, the Host IC with CryptoCompanion, and Reader IC.
PTM Published on: 2011-10-18