Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
ATmega128RFA1-Slide15
As previously discussed, the ATmega128RFA1 offers high data rates up to 2Mbit/s. When designing wireless systems it pays to keep in mind that the effective data rate is smaller than the selected data rate due to the overhead caused by various control signals and checksum computations as defined by the IEEE 802.15.4 standard. The overhead depends further on the length of the Physical layer Service Data Unit (PSDU). Generally the High Data Rate modes offer a higher effective data rate while occupying the same RF channel bandwidth as the IEEE 802.15.4 2.4GHz 250kb/s standard mode. High Data Rate transmission and reception is useful for large PSDU lengths due to the higher effective data rate, further reducing the power consumption of the system.
PTM Published on: 2011-10-18