Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Product List
Analog Devices’ MEMS switches can be used as a substitute for RF Relays in all types of applications, but these first two Analog MEMS Switches are primarily targeting usage in applications in the Automated Test Equipment space. These applications can be broadly broken up into two buckets – one application is switch matrix’s, and the other application bucket is load boards or probe boards, and can also be known as test interface boards. These applications require very low On Leakage for precision measurement, and the ADGM1304 and ADGM1004 are very much on a par with typical RF Relays for this key specification.