Numpad 4000 Mechanical Keyswitch Data Entry Device
2021-12-14 | By Adafruit Industries
License: See Original Project 3D Printing Adafruit Feather Raspberry Pi MCU
Courtesy of Adafruit
Guide by John Park
Overview
Compact keyboards are super cool -- I use a TKL -- but sometimes you just miss having a big, old number pad for data entry and calculations. The Numpad 4000 is just that! Plus, you can move it off to either side of your main keyboard for ideal ergonomics.
You can build the custom mechanical Number Pad of your Dreams with the Ortho NeoKey Snap-Apart PCB, a Feather RP2040, and CircuitPython. Customize the physical layout on this diode-matrixed, NeoPixel-lit wonder board!
Parts
This project should work well on nearly any CircuitPython-capable Feather board. I chose to use the very lovely Feather RP2040.
Key Switches and Keycaps
The NeoKey Ortho 5x6 PCB uses up to 30 keyswitches and key caps, although for the Numpad 4000 you'll only need 22.
Kailh Mechanical Key Switches - Thick Click Jade Box - 10 pack
Kailh Mechanical Key Switches - 10 packs - Cherry MX Compatible
Keycaps
To build the Numpad 4000 as designed here you'll need a set of number pad-specific keys. I used SA profile, double-shot Maxkey keycaps -- these numberpad keys happened to be left over from a TKL (ten key-less) build I did. Talk to a friend who has ordered some fancy keycaps before -- in many cases they'll have left over numpad keys as people tend to make smaller boards!
Or, go for a fully orthographic build using 1u keycaps such as these DSA profile ones:
Little Rubber Bumper Feet - Pack of 4
M2.5 x 18mm Screws x3. These ones from McMaster-Carr are nice.
Tools and Materials
You'll need a 3D printer and filament to build the switch plate and case. Alternately, you can make a variant stacked design using acrylic or wood on a laser cutter or mill, or even with chipboard and a CNC cutter such as the Cricut.
You'll also need a soldering iron, solder, and thin wire such as this:
Silicone Cover Stranded-Core Wire - 30AWG in Various Colors
Numpad Layout
Not all keycaps are square. Keycap ratios are expressed as proportional widths relative to a "one unit", or, "1u" standard, which you find on most of the "normal" alpha-numeric keys on a keyboard.
Other key sizes exist: modifiers are usually 125% width, or 1.25u. Here are some common sizes (these may vary with different designs):
"normal" keys = 1u
alt, ctrl = 1.25u
tab = 1.5u
caps lock = 1.75u
numpad 0, +, enter = 2u
spacebar = 6.25u
Here's a nice resource for learning more about keyboard anatomy, Keyboard University.
Getting Off the Grid
Since this design uses a few 2u keycaps, we'll need to move some of the NeoKey snap-apart PCBs off of the default 1u grid.
The NeoKey Ortho 6x5 Snap-Apart PCB makes it easy to rearrange the layout.
To keep things neat and stable, you can design a key plate for 3D printing, laser cutting, or CNC milling.
An excellent tool for designing your layout in the browser is the Keyboard Layout Editor.
Keyboard Layout Editor
An excellent tool for designing your layout in the browser is the Keyboard Layout Editor.
You can start a new, blank layout, then add keys and rearrange their sizes and positions using the per-key controls.
Using the Keyboard Layout Editor, I created the layout I want.
Once the layout is set, I headed to the Raw Data tab to copy the markup text shown here:
[{c:"#606cc4",t:"#ffffff",p:"DSA",a:5,f:4},"NUM\n\n\n\n\n\nLOCK",{a:7,f:6},"DEL",{f:9},"/","*","-"], [{a:5,f:4},"PAGE\n\n\n\n\n\nUP",{c:"#408dff",a:7,f:9},"7","8","9",{c:"#606cc4",h:2,_s:0},"+"], [{a:5,f:3},"PAGE\n\n\n\n\n\nDOWN",{c:"#408dff",a:7,f:9},"4","5","6"], [{c:"#606cc4",f:6},"FN",{c:"#408dff",f:9},"1","2","3",{c:"#606cc4",f:3,h:2,_s:0},"ENTER"], ["CTRL",{c:"#408dff",f:9,w:2,_s:0},"0","."]
Highlight and copy the markup text so you can use it in the next step.
Note, I added the _s:0 code to remove stabilizer cutouts from the 2u switches.
Plate & Case Builder
Now that you have the keyboard laid out, you can use the swillkb Plate & Case Builder to generate the CAD drawings of your plate layout.
Paste the markup text from the Raw Data you copied in the Keyboard Layout Editor in to the Plate Layout field. Pick and options you want, and then click the Draw My CAD!!! button.
Pick the CAD Output tab and you'll see your drawing.
Click on the file type button to download an SVG, DXF, or EPS file of the drawing. You'll use this in your 3D modeling package of choice, or to generate a laser cutter or CNC toolpath.
Model
Most 3D modeling and CAD programs will allow you to import the drawing file of your choice. I used the venerable .dxf file and imported it into Rhino/Grasshopper.
I then created a Grasshopper workflow to effectively extrude the collection of curves 1.6mm in height to generate the switch plate model. (I also had it offset the outer boundary curve by 2mm and fillet the corners.)
The 1.6mm plate height is a good starting point, allowing the switches to click into place nicely, but you can try making it thicker if you like.
Export the model as an .stl file and 3D print it! (Note, the print shown here was made using the notched keyswitch profile, but the squares work just as well or better due to increased connection surface.)
Assemble the Numpad
Snap
The first step is to snap off the top and bottom of the PCB.
Use some pliers to gently bend at the perforation until the extra material snaps off.
Please use eye protection when breaking apart printed circuit boards.
Extra Column No More
Pry off the extra column at the far right of the board, as seen from the top side of the PCB.
You can save these key PCBs for use in another project later, such as a five-key macro strip!
Snip Snip
Use diagonal cutters to cut off the four key PCBs of the fifth column as shown, taking care to leave the first PCB in place.
Then, snap off two of the four key PCBs you just removed and reserve them for use with the + and ENTER keys later in the build.
You will eventually wire and solder these loose PCBs back into the numpad matrix.
More Snip Snip
Repeat the previous process to turn the bottom row of four into a spaced-out row of three that will accommodate the 2u spacing of the 0 key.
This is the fundamental numpad layout you'll be working with. Next, we'll clean up the board edges.
PCBs contain fiberglass which is hazardous to your health. Wear a facemask when filing or sanding the edges.
Edge Cleanup
Use your diagonal cutters to remove some of the excess material where the boards were separated, then file them down with a small metal file or sandpaper.
Be sure not to breathe in the dust!
3D Case
Use the files linked below and print the plate, top, base, and bottom parts.
Keyswitches, Plate, PCBs
Arrange the PCBs as shown, then snap a few keyswitches into place.
Be careful to align the two metal legs of the keyswitch with the sockets of the PCBs.
One Offs
For the 2u spaced keys, snap the keyswitches through the plate, then press the PCBs on from the back.
Wiring
It's time to wire it all up! There are two sets of wiring tasks here -- one is to connect the key matrix column and row pins to the Feather RP2040 as well as the power, ground, and NeoPixel pin. The other wiring task is to re-connect the snapped-off key PCBs to the others.
Note how the NeoPixel data line runs in a snake-like pattern through the grid.
Follow this wiring diagram to make the connections.
Here the plate and keyswitches have been removed to expose the wiring more clearly.
Note: Sometimes the PCB traces that run between the key PCBs can become damaged when neighboring PCBs have been cut, just due to strain on the thin connection. You can repair these with a short jumper wire as shown on the third PCB on the bottom row in the following photograph.
Assembly
Now that you've wired everything, you can insert all of the keyswitches, and then add the keycaps.
Case Middle
Feed the Feather RP2040 through the case middle section as shown.
Case Top
Place the case top on top of the boards so you can sandwich everything and screw the parts together.
You can start with the three long screws.
Feather Screws, Standoffs
Add the four shorter screws to the Feather mounting holes.
Then, thread the seven hex standoffs onto the screws.
Case Bottom
Set the case bottom in place and then use the smallest screws to attach it to the hex standoffs from below.
You can also add rubber bumper feet as shown for a non-skid experience.
The Numpad 4000 is assembled and ready for coding in CircuitPython.
Install CircuitPython
CircuitPython is a derivative of MicroPython designed to simplify experimentation and education on low-cost microcontrollers. It makes it easier than ever to get prototyping by requiring no upfront desktop software downloads. Simply copy and edit files on the CIRCUITPY drive to iterate.
CircuitPython Quickstart
Follow this step-by-step to quickly get CircuitPython running on your board.
Download the latest version of CircuitPython for this board via circuitpython.org
Click the link above to download the latest CircuitPython UF2 file.
Save it wherever is convenient for you.
To enter the bootloader, hold down the BOOT/BOOTSEL button (highlighted in red above), and while continuing to hold it (don't let go!), press and release the reset button (highlighted in blue above). Continue to hold the BOOT/BOOTSEL button until the RPI-RP2 drive appears!
If the drive does not appear, release all the buttons, and then repeat the process above.
You can also start with your board unplugged from USB, press, and hold the BOOTSEL button (highlighted in red above), continue to hold it while plugging it into USB, and wait for the drive to appear before releasing the button.
A lot of people end up using charge-only USB cables and it is very frustrating! Make sure you have a USB cable you know is good for data sync.
You will see a new disk drive appear called RPI-RP2.
Drag the adafruit_circuitpython_etc.uf2 file to RPI-RP2.
The RPI-RP2 drive will disappear and a new disk drive called CIRCUITPY will appear.
That's it, you're done! :)
Safe Mode
You want to edit your code.py or modify the files on your CIRCUITPY drive but find that you can't. Perhaps your board has gotten into a state where CIRCUITPY is read-only. You may have turned off the CIRCUITPY drive altogether. Whatever the reason, safe mode can help.
Safe mode in CircuitPython does not run any user code on startup and disables auto-reload. This means a few things. First, safe mode bypasses any code in boot.py (where you can set CIRCUITPY read-only or turn it off completely). Second, it does not run the code in code.py. And finally, it does not automatically soft-reload when data is written to the CIRCUITPY drive.
Therefore, whatever you may have done to put your board in a non-interactive state, safe mode gives you the opportunity to correct it without losing all of the data on the CIRCUITPY drive.
Entering Safe Mode in CircuitPython 6.x
This section explains entering safe mode on CircuitPython 6.x.
To enter safe mode when using CircuitPython 6.x, plug in your board or hit reset (highlighted in red above). Immediately after the board starts up or resets, it waits 700ms. On some boards, the onboard status LED (highlighted in green above) will turn solid yellow during this time. If you press reset during that 700ms, the board will start up in safe mode. It can be difficult to react to the yellow LED, so you may want to think of it simply as a slow double click of the reset button. (Remember, a fast double click of reset enters the bootloader.)
Entering Safe Mode in CircuitPython 7.x
This section explains entering safe mode on CircuitPython 7.x.
To enter safe mode when using CircuitPython 7.x, plug in your board or hit reset (highlighted in red above). Immediately after the board starts up or resets, it waits 1000ms. On some boards, the onboard status LED (highlighted in green above) will blink yellow during that time. If you press reset during that 1000ms, the board will start up in safe mode. It can be difficult to react to the yellow LED, so you may want to think of it simply as a slow double click of the reset button. (Remember, a fast double click of reset enters the bootloader.)
In Safe Mode
Once you've entered safe mode successfully in CircuitPython 6.x, the LED will pulse yellow.
If you successfully enter safe mode on CircuitPython 7.x, the LED will intermittently blink yellow three times.
If you connect to the serial console, you'll find the following message.
Auto-reload is off. Running in safe mode! Not running saved code. CircuitPython is in safe mode because you pressed the reset button during boot. Press again to exit safe mode. Press any key to enter the REPL. Use CTRL-D to reload.
You can now edit the contents of the CIRCUITPY drive. Remember, your code will not run until you press the reset button, or unplug and plug in your board, to get out of safe mode.
Flash Resetting UF2
If your board ever gets into a really weird state and doesn't even show up as a disk drive when installing CircuitPython, try loading this 'nuke' UF2 which will do a 'deep clean' on your Flash Memory. You will lose all the files on the board, but at least you'll be able to revive it! After loading this UF2, follow the steps above to re-install CircuitPython.
Download flash erasing "nuke" UF2
Code and use the Numpad 4000
Text Editor
Adafruit recommends using the Mu editor for editing your CircuitPython code. You can get more info in this guide.
Alternatively, you can use any text editor that saves simple text files.
Download the Project Bundle
Your project will use a specific set of CircuitPython libraries and the code.py file, along with a folder full of key configuration files. To get everything you need, click on the Download Project Bundle link below, and uncompress the .zip file.
Drag the contents of the uncompressed bundle directory onto your Feather board's CIRCUITPY drive, replacing any existing files or directories with the same names, and adding any new ones that are necessary.
# SPDX-FileCopyrightText: 2021 John Park for Adafruit Industries # SPDX-License-Identifier: MIT # NUMPAD 4000! Made with snap-apart NeoKey PCB and Feather RP2040. import board import keypad import neopixel import usb_hid from adafruit_hid.keyboard import Keyboard from adafruit_hid.keycode import Keycode COLUMNS = 5 ROWS = 5 BLUE = 0x000510 WHITE = 0x303030 RED = 0xFF0000 board_pix = neopixel.NeoPixel(board.NEOPIXEL, 1, brightness=0.1) board_pix[0] = BLUE key_pixels = neopixel.NeoPixel(board.D5, 30, brightness=0.1) key_pixels.fill(WHITE) keys = keypad.KeyMatrix( row_pins=(board.D4, board.A3, board.A2, board.A1, board.A0), column_pins=(board.D13, board.D12, board.D11, board.D10, board.D9), columns_to_anodes=False, ) kbd = Keyboard(usb_hid.devices) keycode_LUT = [ 0, 1, 2, 3, 4, 5, 6, 7, 8, 10, 11, 12, 13, 14, 15, 16, 17, 18, 20, 21, 23, 24 ] pixel_LUT = [ 0, 1, 2, 3, 4, 8, 7, 6, 5, 10, 11, 12, 13, 14, 18, 17, 16, 15, 20, 21, 23, 24 ] # create a keycode dictionary including modifier state and keycodes keymap = { (0): (0, Keycode.KEYPAD_NUMLOCK), (1): (0, Keycode.BACKSPACE), (2): (0, Keycode.FORWARD_SLASH), (3): (0, Keycode.KEYPAD_ASTERISK), (4): (0, Keycode.KEYPAD_MINUS), (5): (0, Keycode.PAGE_UP), (6): (0, Keycode.KEYPAD_SEVEN), (7): (0, Keycode.KEYPAD_EIGHT), (8): (0, Keycode.KEYPAD_NINE), (9): (0, Keycode.PAGE_DOWN), (10): (0, Keycode.KEYPAD_FOUR), (11): (0, Keycode.KEYPAD_FIVE), (12): (0, Keycode.KEYPAD_SIX), (13): (0, Keycode.KEYPAD_PLUS), (14): (1, Keycode.SHIFT), (15): (0, Keycode.KEYPAD_ONE), (16): (0, Keycode.KEYPAD_TWO), (17): (0, Keycode.KEYPAD_THREE), (18): (2, Keycode.CONTROL), (19): (0, Keycode.KEYPAD_ZERO), (20): (0, Keycode.KEYPAD_PERIOD), (21): (0, Keycode.KEYPAD_EQUALS) # KEYPAD_ENTER on non-mac } shift_mod = False ctrl_mod = False while True: key_event = keys.events.get() if key_event: if key_event.pressed: if keymap[keycode_LUT.index(key_event.key_number)][0] == 1: shift_mod = True elif keymap[keycode_LUT.index(key_event.key_number)][0] == 2: ctrl_mod = True if shift_mod is False and ctrl_mod is False: kbd.press(keymap[keycode_LUT.index(key_event.key_number)][1]) print(keymap[keycode_LUT.index(key_event.key_number)][1]) key_pixels[pixel_LUT.index(key_event.key_number)] = RED elif shift_mod is True and ctrl_mod is False: kbd.press(Keycode.SHIFT, keymap[keycode_LUT.index(key_event.key_number)][1]) print(keymap[keycode_LUT.index(key_event.key_number)][1]) key_pixels[pixel_LUT.index(key_event.key_number)] = RED elif shift_mod is False and ctrl_mod is True: kbd.press(Keycode.CONTROL, keymap[keycode_LUT.index(key_event.key_number)][1]) print(keymap[keycode_LUT.index(key_event.key_number)][1]) key_pixels[pixel_LUT.index(key_event.key_number)] = RED elif shift_mod is True and ctrl_mod is True: kbd.press( Keycode.SHIFT, Keycode.CONTROL, keymap[keycode_LUT.index(key_event.key_number)][1] ) print(keymap[keycode_LUT.index(key_event.key_number)][1]) key_pixels[pixel_LUT.index(key_event.key_number)] = RED board_pix[0] = WHITE if key_event.released: if keymap[keycode_LUT.index(key_event.key_number)][0] == 1: # un-shift shift_mod = False elif keymap[keycode_LUT.index(key_event.key_number)][0] == 2: # un-ctrl ctrl_mod = False kbd.release(keymap[keycode_LUT.index(key_event.key_number)][1]) key_pixels[pixel_LUT.index(key_event.key_number)] = WHITE board_pix[0] = BLUE
Use the Numpad 4000
Once the libraries and code are installed, the Numpad 4000 will work as a USB HID keyboard device. You can try it out right away by plugging the keyboard into your computer via a known good USB cable and then typing in some numbers and symbols.
This guide page has a great intro to CircuitPython HID Keyboard.
For even more details, check out the documentation at https://circuitpython.readthedocs.io/projects/hid/en/latest/ which includes all of the keycodes and media codes you can use.
If you want to customize the keys, to send different keycodes, this dictionary contains all of the mappings:
keymap = { (0): (0, Keycode.KEYPAD_NUMLOCK), (1): (0, Keycode.BACKSPACE), (2): (0, Keycode.FORWARD_SLASH), (3): (0, Keycode.KEYPAD_ASTERISK), (4): (0, Keycode.KEYPAD_MINUS), (5): (0, Keycode.PAGE_UP), (6): (0, Keycode.KEYPAD_SEVEN), (7): (0, Keycode.KEYPAD_EIGHT), (8): (0, Keycode.KEYPAD_NINE), (9): (0, Keycode.PAGE_DOWN), (10): (0, Keycode.KEYPAD_FOUR), (11): (0, Keycode.KEYPAD_FIVE), (12): (0, Keycode.KEYPAD_SIX), (13): (0, Keycode.KEYPAD_PLUS), (14): (1, Keycode.SHIFT), (15): (0, Keycode.KEYPAD_ONE), (16): (0, Keycode.KEYPAD_TWO), (17): (0, Keycode.KEYPAD_THREE), (18): (2, Keycode.CONTROL), (19): (0, Keycode.KEYPAD_ZERO), (20): (0, Keycode.KEYPAD_PERIOD), (21): (0, Keycode.KEYPAD_EQUALS) # KEYPAD_ENTER on non-mac }