Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
ESD-Slide7

Shown on this slide is a lineup of all of Toshiba’s high speed and low capacitance ESD protection diodes. These are meant for applications such as high speed USB3.1, HDMI, Displayport, and RF antennas. Beginning at the left are the industry smallest 01005 packages, followed by the very popular 0201 and 0402 packages. The array packages are shown on the right in various configurations, this slide illustrates the dual and the quad package types.

PTM Published on: 2013-09-24
PTM Updated on: 2017-06-01