Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
LED 23
This slide shows what is contained inside the devices. The functionality can change with one optional resistor, the output can be set or left as fixed and they can be combined to provide different currents as needed. The family includes both high current and low current versions and can dissipate up to 1 W if the PCB is designed to accommodate the thermal performance.
PTM Published on: 2019-01-21