Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
LED 17
In many applications, it is desirable to have circuitry which can be used with legacy phase control TRIAC dimmers. The TS19320CS provides dimming via the phase angle input while preserving power factor correction. There are a wide range of protections built in and the device can be used in either a buck –boost topology or in a flyback mode for maximum flexibility.
PTM Published on: 2019-01-21