Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Product List
The table on this slide focuses on the high-performance parts, organized by power requirement. As can be seen, there are not only low-power but also micro-power and even nano-power parts, which are shown by voltage type: 5, 16, and 36 V. In addition, precision and zero drift components are shown. This refers to changes in voltages over temperature. Also shown are the energy effective parts for the different voltage ranges. These have to do with being energy efficient, but not entirely at the expense of other performance factors. The fast family refers to the frequency of operation. These products are all rail to rail capable and have ESD protection. They are available in small packages.
PTM Published on: 2017-06-22