Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
BP35C5 Evaluation Board Set-up: Step Eight

Once confirmed that all routers are connected, the next step is to look at the routing information. To see this, run the "rplsr" command on the border router. This shows that router 3 and router 2 are connected to the border router, and router 4 is connected to router 3. The connections currently look like the schematic on slide 16. Therefore, the demonstration of the self-forming capability of Wi-SUN technology has been achieved.

PTM Published on: 2023-04-19