Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
BP35C5: Wi-SUN FAN Software Stack

Another reason why the BP35C5 is easy to implement is because it comes with integrated Wi-SUN FAN software. Of course, all this follows the Wi-SUN Alliance IEE802.15.4g standard, so connecting it into the network is a breeze. It already handles features such as frequency hopping, discovery/joining which are self-forming and self-healing properties, and security authentication management. The Wi-SUN FAN embedded software is included from the physical to the MAC layer. In addition, the top layer is an API which can be controlled by using simple commands via UART.

PTM Published on: 2023-04-19