Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Timer-Slide8

The third block contains the 8 channels themselves. Each channel is completely independent, however only even channels can be selected as master channels and the odd channels can only operate as slave channels. Typically each channel has an input, an output and a dedicated control register to set up how the channel should operate. The control register determines if the channel should be used, for example, as an interval timer or in PWM slave mode.

PTM Published on: 2012-04-17