Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Timer-Slide21

The sub count register RSUBC counts the reference time for a one second interval. It counts up to 0x8000 (corresponding to 1 sec @ 32.768kHz) and then increments the Second Count Register by one and so on. Since sub-oscillator crystals are not that accurate and can have a wide drift over temperature range, Renesas has implemented a Watch Error Correction feature. The watch error correction value can be set depending on the temperature. This helps to improve accuracy of the real-time counter by offsetting the inaccuracy of the sub-system clock drift over temperature.

PTM Published on: 2012-04-17