Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
AECLOUD-Slide21

This illustration provides further details on connections between the cellular board and Wi-Fi module. The Wi-Fi module communicates with the S5D9 MCU board through the SPI using the PMOD connector. The cellular board interfaces with the S5D9 MCU board via the Arduino headers using one UART for cellular data and another UART for GPS data. The power management for the cellular board is also handled through the Arduino header.

PTM Published on: 2018-12-11