Therefore, on the next TMR0 interrupt when the contents of the TMR1 registers are read, a smaller value than the previous interrupt should be retrieved. Comparing both values can identify a sensor touch. The frequency difference is exaggerated in the illustration to highlight these changes. In reality, a frequency change of between 1% and 5% can be expected.