Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Product List
Transformer drivers should be considered when a customer is looking to develop an isolated DC-DC power supply, to provide isolated power for applications such as the applications shown on this slide. The customer should then check if their application can utilize an unregulated power supply architecture, to determine if a transformer driver architecture is acceptable.
PTM Published on: 2013-09-25
PTM Updated on: 2014-12-02