Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Product List
Analog Devices' MAX6070 and MAX6071 are the highest performing SOT23 voltage references in the industry. High accuracy and low drift, coupled with superior low-frequency noise allow for SO-8 performance in a small SOT23 package. In this example the MAX6070A is compared to the MAX6161A to show key benefits for the designer in terms of smaller PCB area with improved temperature coefficient and initial accuracy.
PTM Published on: 2015-02-25