Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
digital-power-slide9

Similarly, the DPMs can be negatively biased as well. This allows monitoring of a load circuit’s negative rail. The output of the 3.3V regulator and the input voltage requirements of VCC are referenced to the potential at the ground pin, thus, all digital and alert pins need level shifting to communicate to the MCU that is ground referenced. The circuit displayed here can be used as a reference design for a system with a -12V rail.

PTM Published on: 2016-02-25