Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Product List
MicroModule requires less than 10 mm of mounting depth, allowing it to be easily integrated into tight, cramped spaces. MicroModule is unaffected by mounting orientation: it can be mounted horizontally, as in a desktop keyboard; vertically, as on a machine control panel; or any angle in between. Custom bezels can be fabricated or molded to allow integration into devices such as machine control panels or notebook computers. Care should be taken to avoid inadvertent pressure on the top membrane of the sensor as such pressure could be confused with a user’s external touch. The membrane is supported at its edge by an internal spacer. Parts used to capture the VersaPad® module must not make contact with the sensor inside the electrically active area. When mounting MicroModule, the suggested clearance for the cut-out around the actuator (Finger Disk or Mini-Joystick) is 0.5 mm and 1.0 mm for the click buttons.
PTM Published on: 2013-05-13