Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Product List
The first interface factor to consider is whether the Android platform supports USB host. Android smartphones always provide a USB device port but some Android tablets provide both USB host and USB device ports. The USB device port is for connecting to a PC or embedded host to enable data transfer and battery charging. The USB host port is for connecting to USB peripheral hardware. Many Android platforms are now supplied with On-The-Go (OTG) USB ports, which allow for the USB port to be either a host or a device. Some of these OTG ports will be USB device only and some will offer both USB host and device capabilities. One way to determine if a user’s Android platform supports USB host and/or device is by the cable type. A Micro-AB cable will likely be both USB host and device, whereas a Micro-B cable will indicate USB device only.
PTM Published on: 2013-03-15