Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Product List
The third integration option to use is FTDI’s legacy drivers. FTDI’s VCP driver provides a virtual com port and the standard D2xx driver provides direct access to the USB device through a DLL. Both of these drivers are mutually exclusive and cannot be used at the same time. Like the Java D2xx driver option, the Android platform must have USB host, provide the USB power, and will work with FTDI’s existing bridge chips, modules, and cables. Unlike the Java D2xx driver option, the Android Platform must be “rooted” to install the VCP and legacy D2xx driver. Although available to all Android versions, use of the legacy drivers is only recommended for Android Platform OS before version 3.2. Interface Option 1 or Option 2 are suggested for current Android Platform OS versions.
PTM Published on: 2013-03-15