Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Slide 31
Product List
If a water wash is used, this will require a process sealed switch. Generally wash temperatures are about 150°F or 66°C, and the typical machine wash zones are: pre-wash – wash – wash – rinse – and dry.
PTM Published on: 2011-10-27