Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide31

There are many sources of noise within an amplifier. The equations shown in this slide are used to calculate the effect on the output. The current noise on the inverting input is multiplied by the feedback resistor, which contributes to Johnson noise. Voltage noise on the input has to multiplied by the noise gain, which is (1 + Rf/Rg). Current noise on the non-inverting input is also multiplied by the noise gain. Lastly, Rg and Rp contribute to noise as well. (Rp = parallel combination of Rf & Rg.  Rp compensates for bias current).

PTM Published on: 2009-01-26