所订产品一般在 7-10个工作日 内送达中国,具体时间取决于收货地点。
最低订购金额为人民币 300 元,顺丰快递免运费配送。
当用人民币下单时,按照国际贸易条款 DDP(DigiKey 支付关税、海关费用和当地税款)方式结算。
电汇预付
更多来自全授权合作伙伴的产品
下单后,从合作伙伴发货平均需要时间 1-3 天,也可能产生额外运费。可能另外收取运费。 实际发货时间请留意产品详情页、购物车和结账页面上的说明。
国际贸易结算方式:CPT(交货时支付关税、海关费用和适用 VAT/应付税金)
有关详情,请访问帮助和支持
Adafruit was founded in 2005 by MIT engineer, Limor "Ladyada" Fried. Her goal was to create the best place online for learning electronics and making the best designed products for makers of all ages and skill levels. Adafruit has grown to over 50 employees in the heart of NYC with a 15,000+ sq ft.
Add hundreds of lights to your home or yard with these fantastic Pebble Pixel Nets. Adafruit carries them in a variety of sizes, from 1x1m to 1x6m large, and they are chainable and expandable, so no vision is too big.
The Metro RP2350 makes a perfect little game console. The on-board HSTX combined with a DVI breakout can output to a standard television or computer monitor for the display. The USB host connection makes it easy to take input from a keyboard to control the game.
Make animated wall art, powered by pebble-style LEDs, and controlled by a Mini Sparkle Motion.
This project demonstrates how to build a color sensor detector using the APDS-9960 and the Adafruit Feather ESP32-S2 TFT (you can also use Adafruit Feather ESP32-S3 TFT) to control HomeKit devices through ItsaSNAP.
Each new generation of the Raspberry Pi brings improvements over the last, and the Raspberry Pi 5 is no exception. The new Adafruit Blinka Raspberry Pi5 PioMatter library brings this capability to the Raspberry Pi 5 by way of the PIO peripherals.
This guide will go over using the library as well as covering the examples included with the library.
谢谢!
敬请关注收件箱中的 DigiKey 新闻与更新!
请输入电子邮件地址