Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
2.5 robust
For Swissbit’s 2.5” SSD versions, an aluminum die cast housing is used which is very robust and offers additional good shielding against EMI issues plus a very high thermal dissipation. Swissbit added a thermal conducting pad which connects the controller to the housing and reduces the critical temperature by 5° to 12°C depending on the workload.
PTM Published on: 2017-05-30