Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Product List
In packages with multiple dies, spacing between the die is an important factor. ROHM’s manufacturing capabilities allow for a tighter internal 0.3 mm die spacing. When the distance between the die becomes smaller, there is an improvement in color mixture. As seen on the right, ROHM’s PICOLED-RGB tighter die spacing provides the benefit of wider and richer color mixture.
PTM Published on: 2014-08-29
PTM Updated on: 2018-08-27