Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
symmetric
A symmetric light shape is also a benefit of ROHM’s PICOLED and PICOLED-Eco parts. This slide shows the light shape of a standard LED and a ROHM PICOLED from the top view as if one was looking down at the LED. Shown here, the standard LED on the left has an oval shape due to the rectangular 1 mm x 0.6 mm active area. The ROHM PICOLED and PICOLED-Eco devices have a symmetric shape due to the 0.6 mm x 0.6 mm symmetric active area.
PTM Published on: 2014-08-29
PTM Updated on: 2018-08-27