Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Product List
Let’s look at the I/O levels of the devices. On 5V dsPIC30 devices, the digital inputs can accept input voltages from zero to just over 5V. The analog inputs can also span zero to 5V. And the outputs can also span zero to 5V.
PTM Published on: 2011-11-07