Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Product List
Shown here is a picture of an ultrasound system with its signal path. On the very left, a high voltage multiplexer is being used on the transducer side. A high voltage multiplexer is also highlighted on the bottom of the slide, because it is generally used in the signal path to select probes in many applications. The MAX14866 is used because of its small size and scalability.
PTM Published on: 2018-07-10