Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Image of Laird Thermal Systems Thermoelectric Cooler Assemblies and Temperature Controllers - Slide16

In summary, Thermoelectric Cooler Assemblies are compact cooling units that control the temperature in analytical, medical, industrial, telecom and outdoor applications. Laird Thermal Systems offers a wide range of Thermoelectric Cooler Assemblies designed for specific heat transfer methods, cooling capacity ranges and size constraints. Sizing of the unit is straight forward by matching the performance chart of Thermoelectric Cooler Assembly to the primary attributes specified for an application. Laird Thermal Systems also offers thermostatic or proportional temperature controllers to drive thermoelectric cooler assemblies in closed loop feedback systems.

PTM Published on: 2020-03-05