Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Component Selection Table

In this generic guideline table, a direct relation is presented between the most common power rails and the 10% and 20% derating levels, defined by the series to be used and the mission profile of the application in terms of temperature.

PTM Published on: 2023-02-22