To account for the thermal performance, it is important to consider that all of the thermal resistances are taken into account. The example shown here shows the different level of interfacial resistance that needs to be taken into consideration to determine the thermal performance. Clamping forces at 10% compression on Gap Pad material with TO-220 (heat source) allows the designer to determine the pressure vs thermal impedance.