Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
intro
Welcome to the Future Designs In Circuit Programming for NXP Flash Microcontrollers product training module. FDI has developed a family of PC based support products for ISP (In System Programming) and ICP (In Circuit Programming) of Flash based microcontrollers from NXP. These devices plug into the USB port eliminating the need for external power supplies and use NXP's free Flash Magic PC software to program, erase, and verify the code being used. Each kit comes complete with documentation and any cables needed to interface to the target.
PTM Published on: 2011-09-14