Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Product List
Key highlights to be discussed in further detail include flash and RAM size, EEPROM emulation using the flash, low-power, accurate internal clock source to maximize I/O and reduce system cost by pulling off crystals, and three types of serial communication peripherals, all of which are accessible in 16-pin packages. The QG devices also include a variety of packages, ranging from extremely small 8DFN to easy-to-use 16PDIP. They also have the same powerful TPM modules as other S08s, and an 8-bit modulo timer. They have a very accurate 10-bit ADC and analog comparator and an On-chip ICE and background debug module.
PTM Published on: 2011-10-12