Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
automotive-slide19

Requirements for capacitors being used in the DC/DC converter include very high reliability, vibration resistance, excellent current handling capability, and low ESR. For this application, EPCOS offers two different series, the first is the standard polyester or the MKT B3252. The normal capacitance value required for this position is from 5 to 220µF and the voltage is up to 400 VDC. The other type offered is the DC Link which was discussed on the previous slides. Different lead configurations are available for these types, two pin, four pin, or multi-pin and even flat terminals in some cases. Both of these series offer low ESR at high frequencies and high current capabilities.

PTM Published on: 2012-09-17