Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
automotive-slide18

Since in most of the hybrid drives there is no starter and no alternator, the DC/DC converter must be bi-directional. This makes it possible for the DC/DC converter to be used for the conversion of the battery voltage of 14V to a higher voltage level (42V or higher) and vice versa for applications such as power steering. Shown on this slide is a typical DC/DC converter circuit for a hybrid / electric vehicle. Film capacitors are used as the input and output filter capacitors.

PTM Published on: 2012-09-17