Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PSoC 4000: Low-Cost 32-bit MCU Slide 3

PSoC is the world’s first programmable embedded design platform and features a 32-bit ARM Cortex-M MCU which enables accelerated system design and optimized power consumption. PSoC is a proven and reliable solution that has sold over 1.7 billion units and has been used in various application across segments including industrial, consumer, medical, networking, and automotive. Cypress has invested in PSoC since 2000, rolling out the one-chip solution in 2002 and shipping its one-billionth PSoC unit in 2011. In 2013, Cypress launched the flexible, low-power ARM Cortex-M0 one-chip solution, the PSoC 4. The PSoC 4000 is an extension of the PSoC 4 family.

PTM Published on: 2015-02-10