Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Switch Fundamentals Slide 19

As explained on an earlier slide showing the basic MOSFET structure, the input buffer level shifts the digital inputs and applies signal to the drivers which are responsible for turning on and off the switch channels. As with any digital signal, there are four important specifications known as trigger levels that must be observed to ensure correct operation of the switch. Two of these specifications are V(ih) and V(il). V(ih) is the minimum voltage level required by the input buffer to recognize a logic high. For a logic low, V(il) is the maximum voltage level that can be applied to the input buffer to ensure a logic low, while 0V is the minimum acceptable voltage. In order to meet the V(il) and V(ih) levels of the switch, it is important that the designer considers the output voltage levels of the device driving/controlling the switch. The output levels of that preceding device driving the switch are known as V(oh) and V(ol). V(oh) is the minimum voltage level that the preceding device will output as a logic high. This level must exceed the V(ih) requirement of the switch. On the other-hand, V(ol) is the maximum level that the preceding device will output as a logic low, and this voltage level must be less than the V(il) requirements of the switch.

PTM Published on: 2009-07-13