Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
clipKIT-Slide11

To install a clipKIT™ superGRIP™ assembly first place the frame clip around two corners of the component on the board. The frame clip will bend slightly at the “horseshoe” tab. Then press opposite ends of the frame clip down until it is secure around the component’s edges. Make sure the fit is secure by pushing the spread slightly apart at the “horseshoe” tabs while at the same time pressing down on the frame clip.

PTM Published on: 0215-05-27