Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Laminating-Slide5

As can be seen in the graphic, the 3M adhesive 200MP has a very good performance and the 3M adhesive 100MP has the best performance in this category. The 3M adhesive 200MP has been the benchmark in the industry for 30 plus years. It is used for graphic attachment, plastic die cut attachment and lens attachment for LCD displays. The 3M adhesive 100MP has higher temperature resistance and is used for metal, flex circuit, and PCB LED attachment. Both adhesive families offer outstanding adhesion to metal and high surface energy plastics.

PTM Published on: 2011-10-13