Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Laminating-Slide12

An adhesive that maintains integrity and performance when exposed to a diverse range of environmental conditions is extremely important for the end user. The 3M adhesive 100MP has a short term temperature resistance of up to 500°F with no degradation over time. Both the 3M adhesive 100MP and 200MP families have excellent long term holding power at elevated temperature. The shear holding values are dependent on load and temperature, but will hold longer than 10,000 minutes with a high performance acrylic pressure sensitive adhesive. (7514 and 7533 are 3M's screen printable adhesives.)

PTM Published on: 2011-10-13