制造商零件编号 LTC7801EFE#TRPBF
IC REG CTRLR SYNC BUCK 24TSSOP
Analog Devices Inc.
所订产品一般在 7-10个工作日 内送达中国,具体时间取决于收货地点。
最低订购金额为人民币 300 元,顺丰快递免运费配送。
当用人民币下单时,按照国际贸易条款 DDP(DigiKey 支付关税、海关费用和当地税款)方式结算。
电汇预付
更多来自全授权合作伙伴的产品
下单后,从合作伙伴发货平均需要时间 1-3 天,也可能产生额外运费。可能另外收取运费。 实际发货时间请留意产品详情页、购物车和结账页面上的说明。
国际贸易结算方式:CPT(交货时支付关税、海关费用和适用 VAT/应付税金)
有关详情,请访问帮助和支持
Two more components need to be selected for the Arduino/MBed Power Supply Design: an output voltage sensor and an inductor current sensor. The output of these sensors is necessarily dependent on the controller that will use the signals. Based on our synchronous topology, ~15V input and 3.3V output, and the 10V gate-source threshold voltage of the MOSFETs, the Analog Devices LTC7801 will work. This chip requires both inductor current and output voltage feedback. The chip's datasheet tells us how the chip wants these signals presented to it.
The inductor current can be sensed by adding a small resistor, a current-sense resistor, in series with the inductor, between it and the output capacitor. The LTC7801 has two pins, Sense+ and Sense-, that measure the voltage across the resistor to determine the current.
The value of the sense resistor determines the maximum average inductor current that the regulator will allow. We want 0.5A nominal with 0.05A ripple through the inductor at most, so the sense resistor should be sized to be
Vsense(max) comes from the datasheet and is 66mV. Rsense should thus be 120mΩ.
The output voltage can be sensed using a resistor divider between the output rail and ground, with Vfb connected to the center point. The datasheet provides an equation to determine the two resistors, Ra and Rb, of the divider to get the chip to regulate to a desired output voltage. Rb is the resistor connected to the output rail (the 511kΩ above), and Ra is connected to ground (the 36.5kΩ above).
We want an output voltage of 3.3V, so the ratio of our resistances must be
or 3.125. To minimize the power dissipated in the voltage-sensing resistor divider, the resistance of each component should be large. For simplicity, Rb = 312.5kΩ, Ra = 100kΩ.
We've now provided our control chip with the means to read both output voltage and inductor current. Most importantly, the signals are in a format the controller can understand and can use to ensure stable operation. The signals were provided using a current sense resistor and an output voltage divider network. The controller will use these signals to switch the converter such that a constant 3.3V output to our microcontroller is maintained.
谢谢!
敬请关注收件箱中的 DigiKey 新闻与更新!
请输入电子邮件地址