制造商零件编号 U001-C
ENV III UNIT WITH TEMPERATURE HU
M5Stack Technology Co., Ltd.
License: General Public License Wifi Arduino M5Stack
* Thanks for the source code and project information provided by @Huixiang Wee
Story
Driving question: How can we make up for the lack of manpower in the agricultural sector.
The agricultural sector faces a lack of manpower, and we want to use the m5stack to reduce the need of manpower by using it to detect hardware errors
main flowchart and rfid security flow chart
sensor and alarm flow chart
youtube link:
Code
Smart Alarm System For Indoor Agriculture Python
An alarm will sound when there is a significant deviation between expected values and sensor values. or if the system cannot correct minor deviations in value. It will also suggest possible hardware errors that could cause the error.
from m5stack import *
from m5ui import *
from uiflow import *
import time
import unit
setScreenColor(0x222222)
env2_1 = unit.get(unit.ENV2, unit.PAHUB0)
light_1 = unit.get(unit.LIGHT, unit.PORTB)
rfid_1 = unit.get(unit.RFID, unit.PAHUB1)
pahub_0 = unit.get(unit.PAHUB, unit.PORTA)
sensors = None
light = None
moisture_error = None
Temp_error = None
light_error = None
error_level = None
Temperature = None
rfid_time = None
security = None
alarm_off = None
temp_Time = None
error = None
Aircon = None
i = None
moisture = None
Light_time = None
card = None
aircon = M5TextBox(10, 10, "Air-con temp:", lcd.FONT_Default, 0xFFFFFF, rotate=0)
aircon_temp = M5TextBox(120, 10, "Text", lcd.FONT_Default, 0xFFFFFF, rotate=0)
temp = M5TextBox(10, 35, "Temperature: ", lcd.FONT_Default, 0xFFFFFF, rotate=0)
Temp_data = M5TextBox(120, 35, "Text", lcd.FONT_Default, 0xFFFFFF, rotate=0)
light_label = M5TextBox(10, 60, "Light:", lcd.FONT_Default, 0xFFFFFF, rotate=0)
Light_Data = M5TextBox(120, 60, "Text", lcd.FONT_Default, 0xFFFFFF, rotate=0)
test2 = M5TextBox(120, 110, "Text", lcd.FONT_Default, 0xFFFFFF, rotate=0)
test1 = M5TextBox(10, 110, "Text", lcd.FONT_Default, 0xFFFFFF, rotate=0)
humidity = M5TextBox(10, 85, "humidity", lcd.FONT_Default, 0xFFFFFF, rotate=0)
humidity_data = M5TextBox(120, 85, "Text", lcd.FONT_Default, 0xFFFFFF, rotate=0)
rfid_text = M5TextBox(135, 135, "Text", lcd.FONT_Default, 0xFFFFFF, rotate=0)
broken_aircon = M5TextBox(200, 35, "Broken air-con", lcd.FONT_Default, 0xffffff, rotate=0)
broken_light = M5TextBox(200, 60, "Broken light", lcd.FONT_Default, 0xffffff, rotate=0)
s1 = M5TextBox(10, 135, "security status", lcd.FONT_Default, 0xFFFFFF, rotate=0)
alarm = M5TextBox(41, 224, "alarm", lcd.FONT_Default, 0x33cc00, rotate=0)
from numbers import Number
# Describe this function...
def moisture_detect():
global sensors, light, moisture_error, Temp_error, light_error, error_level, Temperature, rfid_time, security, alarm_off, temp_Time, error, Aircon, i, moisture, Light_time, card
if moisture + 5 < (env2_1.humidity) or moisture - 5 > (env2_1.humidity):
moisture_error = 2
elif moisture + 2 < (env2_1.humidity):
if 0 <= 30:
moisture_error = 1
elif 0 > 30:
moisture_error = 2
elif moisture - 2 > (env2_1.humidity):
if 0 <= 30:
moisture_error = 1
elif 0 > 30:
moisture_error = 2
else:
moisture_error = 0
# Describe this function...
def Temp_detect():
global sensors, light, moisture_error, Temp_error, light_error, error_level, Temperature, rfid_time, security, alarm_off, temp_Time, error, Aircon, i, moisture, Light_time, card
if Temperature + 5 < (env2_1.temperature) or Temperature - 5 > (env2_1.temperature):
broken_aircon.show()
Temp_error = 2
elif Temperature + 2 < (env2_1.temperature):
if temp_Time <= 30:
temp_Time = (temp_Time if isinstance(temp_Time, Number) else 0) + 1
Temp_error = 1
elif temp_Time > 30:
Temp_error = 2
elif Temperature - 2 > (env2_1.temperature):
if temp_Time <= 30:
temp_Time = (temp_Time if isinstance(temp_Time, Number) else 0) + 1
Temp_error = 1
elif temp_Time > 30:
Temp_error = 2
broken_aircon.show()
else:
Temp_error = 0
temp_Time = 0
if temp_Time % 5 == 0 and temp_Time > 0:
if temp_Time <= 30:
if Temperature + 2 < (env2_1.temperature):
Aircon = (Aircon if isinstance(Aircon, Number) else 0) + -1
elif Temperature - 2 > (env2_1.temperature):
Aircon = (Aircon if isinstance(Aircon, Number) else 0) + 1
# Describe this function...
def light_detect():
global sensors, light, moisture_error, Temp_error, light_error, error_level, Temperature, rfid_time, security, alarm_off, temp_Time, error, Aircon, i, moisture, Light_time, card
if light + 200 < (light_1.analogValue):
light_error = 2
elif light - 200 > (light_1.analogValue):
light_error = 2
broken_light.show()
else:
light_error = 0
broken_light.hide()
# Describe this function...
def error_lvl():
global sensors, light, moisture_error, Temp_error, light_error, error_level, Temperature, rfid_time, security, alarm_off, temp_Time, error, Aircon, i, moisture, Light_time, card
sensors = [light_error, Temp_error, moisture_error]
error_level = 0
for error in sensors:
if error == 2 or error_level == 2:
rgb.setColorAll(0xff0000)
error_level = 2
break
elif error == 1 or error_level == 1:
rgb.setColorAll(0xff6600)
error_level = 1
break
else:
error_level = 0
rgb.setColorAll(0x33cc00)
if error_level == 2:
if alarm_off == False:
speaker.tone(1800, 200)
else:
wait_ms(200)
else:
wait_ms(200)
# Describe this function...
def home_screen():
global sensors, light, moisture_error, Temp_error, light_error, error_level, Temperature, rfid_time, security, alarm_off, temp_Time, error, Aircon, i, moisture, Light_time, card
if light_error == 2:
Light_Data.setColor(0xff0000)
elif light_error == 0:
Light_Data.setColor(0xffffff)
if moisture_error == 2:
humidity_data.setColor(0xff0000)
elif moisture_error == 1:
humidity_data.setColor(0xff6600)
elif moisture_error == 0:
humidity_data.setColor(0xffffff)
if Temp_error == 2:
Light_Data.setColor(0xff0000)
broken_aircon.show()
elif Temp_error == 1:
Temp_data.setColor(0xff6600)
elif Temp_error == 0:
Temp_data.setColor(0xffffff)
broken_aircon.hide()
# Describe this function...
def variableSet():
global sensors, light, moisture_error, Temp_error, light_error, error_level, Temperature, rfid_time, security, alarm_off, temp_Time, error, Aircon, i, moisture, Light_time, card
light = 800
Temperature = 24
Aircon = 22
temp_Time = 0
Light_time = 0
error_level = 0
moisture = 71
security = False
alarm_off = False
rfid_time = 0
# Describe this function...
def rfid():
global sensors, light, moisture_error, Temp_error, light_error, error_level, Temperature, rfid_time, security, alarm_off, temp_Time, error, Aircon, i, moisture, Light_time, card
if rfid_1.isCardOn():
if rfid_1.isCardOn():
for i in ['32ff5d1282', '32ff5d9082', '324e5d1582']:
if (rfid_1.readUid()) == i:
card = True
break
else:
card = False
if card == True:
security = True
rfid_time = 0
else:
security = False
elif rfid_time <= 10:
rfid_time = (rfid_time if isinstance(rfid_time, Number) else 0) + 1
elif rfid_time > 10:
security = False
else:
security = False
def buttonA_wasPressed():
global sensors, light, moisture_error, Temp_error, light_error, error_level, Temperature, rfid_time, security, alarm_off, temp_Time, Aircon, moisture, Light_time, card, i, error
if security == True:
if alarm_off == False:
alarm_off = True
alarm.setColor(0xff0000)
elif security == True:
alarm_off = False
alarm.setColor(0x33cc00)
pass
btnA.wasPressed(buttonA_wasPressed)
speaker.setVolume(0)
rgb.setBrightness(10)
pahub_0.select(0, 1)
pahub_0.select(1, 1)
broken_light.hide()
broken_aircon.hide()
variableSet()
while True:
rfid()
moisture_detect()
Temp_detect()
light_detect()
error_lvl()
home_screen()
aircon_temp.setText(str(Aircon))
Temp_data.setText(str(env2_1.temperature))
Light_Data.setText(str(light_1.analogValue))
humidity_data.setText(str(env2_1.humidity))
test2.setText(str(temp_Time))
test1.setText(str(sensors))
rfid_text.setText(str(security))
wait_ms(800)
wait_ms(2)
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.
Visit TechForum