制造商零件编号 4500
CLUE NRF52840 EXPRESS
Adafruit Industries LLC
License: See Original Project Humidity Light Movement Sound Temperature
Courtesy of Adafruit
Guide by Liz Clark
Overview
The CLUE has tons of onboard sensors that can sense movement, light, sound, and environmental measures like temperature and humidity. This project uploads code to the CLUE using PyLeap that uses the CLUE's onboard display to plot all of the sensors' data.
This project was originally created by Kevin Walters. The original Learn Guide can be found here.
Original CLUE Sensor Plotter in CircuitPython Learn Guide
Parts
Clear Acrylic Enclosure + Hardware Kit for Adafruit CLUE
3 x AA Battery Holder with On/Off Switch, JST, and Belt Clip
Text editor powered by tinymce.
CircuitPython on CLUE
CircuitPython is a derivative of MicroPython designed to simplify experimentation and education on low-cost microcontrollers. It makes it easier than ever to get prototyping by requiring no upfront desktop software downloads. Simply copy and edit files on the CIRCUITPY flash drive to iterate.
The following instructions will show you how to install CircuitPython. If you've already installed CircuitPython but are looking to update it or reinstall it, the same steps work for that as well!
Set up CircuitPython Quick Start!
Follow this quick step-by-step for super-fast Python power :)
Download the latest version of CircuitPython for CLUE from circuitpython.org
Click the link above to download the latest version of CircuitPython for the CLUE.
Download and save it to your desktop (or wherever is handy).
Plug your CLUE into your computer using a known-good USB cable.
A lot of people end up using charge-only USB cables and it is very frustrating! So, make sure you have a USB cable you know is good for data sync.
Double-click the Reset button on the top (magenta arrow) on your board, and you will see the NeoPixel RGB LED (green arrow) turn green. If it turns red, check the USB cable, try another USB port, etc. Note: The little red LED next to the USB connector will pulse red. That's ok!
If double-clicking doesn't work the first time, try again. Sometimes it can take a few tries to get the rhythm right!
You will see a new disk drive appear called CLUEBOOT.
Drag the adafruit-circuitpython-clue-etc.uf2 file to CLUEBOOT.
The LED will flash. Then, the CLUEBOOT drive will disappear, and a new disk drive called CIRCUITPY will appear.
If this is the first time, you're installing CircuitPython or you're doing a completely fresh install after erasing the filesystem, you will have two files - boot_out.txt, and code.py, and one folder - lib on your CIRCUITPY drive.
If CircuitPython was already installed, the files present before reloading CircuitPython should still be present on your CIRCUITPY drive. Loading CircuitPython will not create new files if there was already a CircuitPython filesystem present.
That's it, you're done! :)
Text editor powered by tinymce.
Pairing
Now that you're done uploading the correct firmware, disconnect your device from your computer and power it via Li-Poly or AAA battery pack.
Pairing device to PyLeap
Once powered, press the small Reset button in the center of the board (Circuit Playground Bluefruit) or on the top right of the board (CLUE). When the blue light flashes, press the Reset button again.
Circuit Playground Bluefruit with a small Reset button in the center of the board
Adafruit CLUE Reset Button (Highlighted on the upper right)
When done correctly, the LEDs will flash yellow followed by solid blue. Once this occurs, the board will continuously be in discovery mode.
Scan & Connect
When your Circuit Playground Bluefruit or Adafruit CLUE is in discovery mode, hold it very closely to your iPhone or iPadOS to pair.
Below the spinning Blinka, you'll notice a status indicator that will let you know your current pairing status.
Once you've found your device and received the Bluetooth Pairing Request message, press Pair to pair your board to your iPhone or iPadOS.
If your Circuit Playground Bluefruit doesn't appear:
Check to see if your Circuit Playground Bluefruit is powered on. Verify that the green On light is lit.
Make sure your Circuit Playground Bluefruit is running the correct firmware. See the CircuitPython page in this guide.
Try resetting the Circuit Playground Bluefruit by pressing the small Reset button near the center of the board.
Text editor powered by tinymce.
Sensor Plotter Code
# SPDX-FileCopyrightText: 2020 Kevin J Walters for Adafruit Industries
#
# SPDX-License-Identifier: MIT
# clue-plotter v1.14
# Sensor and input plotter for Adafruit CLUE in CircuitPython
# This plots the sensors and three of the analogue inputs on
# the LCD display either with scrolling or wrap mode which
# approximates a slow timebase oscilloscope, left button selects
# next source or with long press changes palette or longer press
# turns on output for Mu plotting, right button changes plot style
# Tested with an Adafruit CLUE (Alpha) and CircuitPython and 5.0.0
# copy this file to CLUE board as code.py
# needs companion plot_sensor.py and plotter.py files
# MIT License
# Copyright (c) 2020 Kevin J. Walters
# Permission is hereby granted, free of charge, to any person obtaining a copy
# of this software and associated documentation files (the "Software"), to deal
# in the Software without restriction, including without limitation the rights
# to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
# copies of the Software, and to permit persons to whom the Software is
# furnished to do so, subject to the following conditions:
# The above copyright notice and this permission notice shall be included in all
# copies or substantial portions of the Software.
# THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
# IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
# FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
# AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
# LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
# OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
# SOFTWARE.
import time
import gc
import board
from adafruit_clue import clue
from plotter import Plotter
# pylint: disable=unused-import
from plot_source import (
PlotSource,
TemperaturePlotSource,
PressurePlotSource,
HumidityPlotSource,
ColorPlotSource,
ProximityPlotSource,
IlluminatedColorPlotSource,
VolumePlotSource,
AccelerometerPlotSource,
GyroPlotSource,
MagnetometerPlotSource,
PinPlotSource,
)
debug = 1
# A list of all the data sources for plotting
# NOTE: Due to memory contraints, the total number of data sources
# is limited. Can try adding more until a memory limit is hit. At that
# point, decide what to keep and what to toss. Can comment/uncomment lines
# below as desired.
sources = [
TemperaturePlotSource(clue, mode="Celsius"),
# TemperaturePlotSource(clue, mode="Fahrenheit"),
PressurePlotSource(clue, mode="Metric"),
# PressurePlotSource(clue, mode="Imperial"),
HumidityPlotSource(clue),
ColorPlotSource(clue),
ProximityPlotSource(clue),
# IlluminatedColorPlotSource(clue, mode="Red"),
# IlluminatedColorPlotSource(clue, mode="Green"),
# IlluminatedColorPlotSource(clue, mode="Blue"),
# IlluminatedColorPlotSource(clue, mode="Clear"),
# VolumePlotSource(clue),
AccelerometerPlotSource(clue),
# GyroPlotSource(clue),
# MagnetometerPlotSource(clue),
# PinPlotSource([board.P0, board.P1, board.P2])
]
# The first source to select when plotting starts
current_source_idx = 0
# The various plotting styles - scroll is currently a jump scroll
stylemodes = (
("lines", "scroll"), # draws lines between points
("lines", "wrap"),
("dots", "scroll"), # just points - slightly quicker
("dots", "wrap"),
)
current_sm_idx = 0
def d_print(level, *args, **kwargs):
"""A simple conditional print for debugging based on global debug level."""
if not isinstance(level, int):
print(level, *args, **kwargs)
elif debug >= level:
print(*args, **kwargs)
def select_colors(plttr, src, def_palette):
"""Choose the colours based on the particular PlotSource
or forcing use of default palette."""
# otherwise use defaults
channel_colidx = []
palette = plttr.get_colors()
colors = PlotSource.DEFAULT_COLORS if def_palette else src.colors()
for col in colors:
try:
channel_colidx.append(palette.index(col))
except ValueError:
channel_colidx.append(PlotSource.DEFAULT_COLORS.index(col))
return channel_colidx
def ready_plot_source(plttr, srcs, def_palette, index=0):
"""Select the plot source by index from srcs list and then setup the
plot parameters by retrieving meta-data from the PlotSource object."""
src = srcs[index]
# Put the description of the source on screen at the top
source_name = str(src)
d_print(1, "Selecting source:", source_name)
plttr.clear_all()
plttr.title = source_name
plttr.y_axis_lab = src.units()
# The range on graph will start at this value
plttr.y_range = (src.initial_min(), src.initial_max())
plttr.y_min_range = src.range_min()
# Sensor/data source is expected to produce data between these values
plttr.y_full_range = (src.min(), src.max())
channels_from_src = src.values()
plttr.channels = channels_from_src # Can be between 1 and 3
plttr.channel_colidx = select_colors(plttr, src, def_palette)
src.start()
return (src, channels_from_src)
def wait_release(func, menu):
"""Calls func repeatedly waiting for it to return a false value
and goes through menu list as time passes.
The menu is a list of menu entries where each entry is a
two element list of time passed in seconds and text to display
for that period.
The entries must be in ascending time order."""
start_t_ns = time.monotonic_ns()
menu_option = None
selected = False
for menu_option, menu_entry in enumerate(menu):
menu_time_ns = start_t_ns + int(menu_entry[0] * 1e9)
menu_text = menu_entry[1]
if menu_text:
plotter.info = menu_text
while time.monotonic_ns() < menu_time_ns:
if not func():
selected = True
break
if menu_text:
plotter.info = ""
if selected:
break
return (menu_option, (time.monotonic_ns() - start_t_ns) * 1e-9)
def popup_text(plttr, text, duration=1.0):
"""Place some text on the screen using info property of Plotter object
for duration seconds."""
plttr.info = text
time.sleep(duration)
plttr.info = None
mu_plotter_output = False
range_lock = False
initial_title = "CLUE Plotter"
# displayio has some static limits on text - pre-calculate the maximum
# length of all of the different PlotSource objects
max_title_len = max(len(initial_title), max([len(str(so)) for so in sources]))
plotter = Plotter(
board.DISPLAY,
style=stylemodes[current_sm_idx][0],
mode=stylemodes[current_sm_idx][1],
title=initial_title,
max_title_len=max_title_len,
mu_output=mu_plotter_output,
debug=debug,
)
# If set to true this forces use of colour blindness friendly colours
use_def_pal = False
clue.pixel[0] = clue.BLACK # turn off the NeoPixel on the back of CLUE board
plotter.display_on()
# Using left and right here in case the CLUE is cased hiding A/B labels
popup_text(
plotter,
"\n".join(
[
"Button Guide",
"Left: next source",
" 2secs: palette",
" 4s: Mu plot",
" 6s: range lock",
"Right: style change",
]
),
duration=10,
)
count = 0
while True:
# Set the source and start items
(source, channels) = ready_plot_source(
plotter, sources, use_def_pal, current_source_idx
)
while True:
# Read data from sensor or voltage from pad
all_data = source.data()
# Check for left (A) and right (B) buttons
if clue.button_a:
# Wait for button release with time-based menu
opt, _ = wait_release(
lambda: clue.button_a,
[
(2, "Next\nsource"),
(4, ("Source" if use_def_pal else "Default") + "\npalette"),
(6, "Mu output " + ("off" if mu_plotter_output else "on")),
(8, "Range lock\n" + ("off" if range_lock else "on")),
],
)
# pylint: disable=no-else-break
if opt == 0: # change plot source
current_source_idx = (current_source_idx + 1) % len(sources)
break # to leave inner while and select the new source
elif opt == 1: # toggle palette
use_def_pal = not use_def_pal
plotter.channel_colidx = select_colors(plotter, source, use_def_pal)
elif opt == 2: # toggle Mu output
mu_plotter_output = not mu_plotter_output
plotter.mu_output = mu_plotter_output
else: # toggle range lock
range_lock = not range_lock
plotter.y_range_lock = range_lock
if clue.button_b: # change plot style and mode
current_sm_idx = (current_sm_idx + 1) % len(stylemodes)
(new_style, new_mode) = stylemodes[current_sm_idx]
wait_release(lambda: clue.button_b, [(2, new_style + "\n" + new_mode)])
d_print(1, "Graph change", new_style, new_mode)
plotter.change_stylemode(new_style, new_mode)
# Display it
if channels == 1:
plotter.data_add((all_data,))
else:
plotter.data_add(all_data)
# An occasional print of free heap
if debug >= 3 and count % 15 == 0:
gc.collect() # must collect() first to measure free memory
print("Free memory:", gc.mem_free())
count += 1
source.stop()
plotter.display_off()
Text editor powered by tinymce.
Usage
After pairing your CLUE with the PyLeap app, scroll down to the PyLeap CLUE Sensor Plotter project in the list. Tap to open it and then tap on Run it! to download the project to your CLUE over BLE.
Once the project is uploaded, the code will begin running. First, you'll see a "button guide" on the screen that tells you what the CLUE's A and B buttons do. The A button has a few different functions depending on the length of time that you press the button.
Short press: advance to the next sensor
Two seconds: change the palette (colors on the display)
Three seconds: opens the Mu plotter if your CLUE is connected via USB to Mu
Four seconds: locks the range of the plot
The B button changes the style of the plot. You can choose between plotting with a line or dots and having the plotter scroll or wrap.
Toggle through plotting the different sensors on the CLUE. As the sensors' values change, you'll see the onscreen plot change as well.
Going Further
If you're curious about what makes the code tick, or plot, you can check out the original Learn Guide by Kevin Walters. It goes into depth on how everything is working.
Original CLUE Sensor Plotter in CircuitPython Learn Guide
Text editor powered by tinymce.