Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
HVArc Guard Surface Mount MLCC Slide 16

A simple passive R-C snubber is used in power circuitry to dissipate energy and clamp voltages during turn-on and turn-off cycles. For example, in an application where high-voltage MOSFETs are used as the switching device, rapid changes occur as the drain-to-source voltage steps up during MOSFET operation. These changes create voltage transient noise on the gate of the MOSFET. A capacitor snubber is used across the source-drain as a bypass cap for the harmful switching noise. Used in this application, HVArc Guard® capacitor MLCCs will typically require significantly less space than standard high-voltage capacitors. Shown here is an example of a snubber used in a totem pole configured MOSFET circuit. A wide range of passive devices can be used to make a passive snubber that absorbs the energy from the reactance in a power switching circuit. Snubbers can be used to clamp ringing noise, reduce power dissipation during turn-off, or reduce peak switching voltages. Snubbers are a critical circuit for improving the efficiency of most switching semiconductor circuits.

PTM Published on: 2011-11-11