The next step is to connect the third internal supervisor, SVS3. The first two supervisors control rails one and two, the third can be used to monitor the input voltage for any glitches coming in from the source. When SVS3 is not being used it is connected as shown in the diagram on this slide.