Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Product List
The LM3406 also supports a wide input voltage range of up to 75V Input/Output allowing multiple LEDs to be driven in series from one LED driver. Similar fault protection and indication features to the LM3421/23 also protect and extend the lifetime of the LEDs. The LM3406 buck regulator additionally generates up to 96% peak efficiency levels. This is important since high-brightness LEDs can require more than 1W of power and generate a lot of heat. Failure to control thermals can significantly degrade the lifetime and performance of the LEDs. Improving efficiency levels, however, is one way of improving the overall thermal performance of the device, as this minimizes loss in the form of heat.
PTM Published on: 2011-11-03