Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
High Spped Amplifiers for Video Applications Slide 12

So the parameters of importance are bandwidth, slew rate, Diff Gain/Diff Phase in the case of NTSC or PAL video, and to some lesser extent output current capability, power dissipation, operating supplies, etc. Here is a list of parts with these characteristics in mind. As you can see, both CFB and VFB devices have been shown as they are both suitable for these applications. Also other devices, such as Programmable Gain Buffers, Closed Loop Buffers, etc. are also included for completeness. Most of these devices are manufactured on TI’s VIP10 process which has trench isolation between transistors thereby improving speed by lowering capacitance especially at lower operating supply voltages.

PTM Published on: 2011-11-02