Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
H48 Product Range Slide 22

A commonly asked question is whether the H48-2 series can be reworked. With care, all parts of this series can be reworked. However, T-Global strongly recommends that the pads are replaced after use, as this prevents contamination. Another frequently asked question is the shelf life of the product. The shelf life of all gap fillers without an adhesive layer is two years. For gap pads with an adhesive, this is reduced to one year. Also commonly discussed is if the the pads soften with temperature. Up to the maximum working temperature, as specified on the individual product datasheet, the materials will not suffer with temperature increase.

PTM Published on: 2012-04-09
PTM Updated on: 2015-06-19